Skip to main content
Knowledgebase
Home
Renesas Electronics Europe - Knowledgebase

How to change the version of the compiler with a CubeSuite+ project?

Latest Updated:01/20/2015

Question:

How do I change the version number of the compiler for use with a CubeSuite+ project?

Answer:

Select the [Common Options] tabbed page on the [Property] panel for the build tool. Select [Using compiler package version] under the [Version Select] category.
Since the setting [Always latest version which was installed] is selected by default, the version number of the compiler for use with projects is automatically changed when the version of CubeSuite+ or the compiler is updated.

You can change or fix the version of the compiler to be used by specifying a version number as described above.

Suitable Products
CS+ (formerly CubeSuite+)