Skip to main content
Knowledgebase
Home
Renesas Electronics Europe - Knowledgebase

Functions and Variables Access Table

Last Updated:04/17/2017

Question:

What is the Functions and Variables Access Table?

Answer:

It displays the functions that access variables in the form of an orthogonal table.
  When the microcontroller used is a single-core product of RH850, start the exclusive control check tool to check if exclusive control for variables is being performed correctly. This allows you to see the variables in red where exclusive control is not working.

Note: Do not sort the data of the table when starting the exclusive control check tool. The variables not to be checked may be displayed in red too.

Applicable Products: CS+ V4.00.00 and V4.00.01

Suitable Products
CS+ (formerly CubeSuite+)