Error message: CC-RX compiler V. 2: relocation size overflow
Latest Updated:10/29/2014
Question:
When I use the CC-RX compiler V. 2, it produces the following error message. What should I do about it?
E0562330: Relocation size overflow : "file name.obj"-"section name"-"00000025"
Answer:
This message is output if the branch width from "file name.obj" will be illegal.
In [Property] of the CC-RX (build tool), change the setting on the [Common Options] tabbed page to [CPU] -> [Branch width size] -> [Not specified (-branch=32)] (the default setting is [Compiles within 24 bits (-branch=24)]).
In [Property] of the CC-RX (build tool), change the setting on the [Common Options] tabbed page to [CPU] -> [Branch width size] -> [Not specified (-branch=32)] (the default setting is [Compiles within 24 bits (-branch=24)]).
Suitable Products
CS+ (formerly CubeSuite+) |
C/C++ Compiler Package for RX Family |