Skip to main content
Knowledgebase
Home
Renesas Electronics Europe - Knowledgebase

Does extra settings necessary to define interrupt functions?

Latest Updated:04/24/2015

Question:

I am using the CC-RL compiler for RL78 devices. I have attempted to define interrupt functions in the C language but the interrupt request names are not being accepted. Do I need to make some extra settings?

Answer:

Creating a project in an IDE produces an iodefine.h file in which interrupt request names are defined. Include iodefine.h in the C source file you are using to define the functions.
Suitable Products
e² studio
CS+ (formerly CubeSuite+)
C Compiler Package for RL78 Family