Skip to main content
Knowledgebase
Home
Renesas Electronics Europe - Knowledgebase

Do I need to specify the allocation of section to particular addresses?

Latest Updated:04/24/2015

Question:

I am using the CC-RL compiler for RL78 devices. What do I need to do to specify the allocation of sections to particular addresses?

Answer:

Use the linker option –STARt to allocate sections.

Example:
.const,.text,.data,.sdata,.textf,.constf/02000,.dataR,.bss,.stack_bss/FEF00,.sdataR,.sbss/FFE20

Suitable Products
e² studio
CS+ (formerly CubeSuite+)
C Compiler Package for RL78 Family