Skip to main content
Knowledgebase
Home
Renesas Electronics Europe - Knowledgebase

CubeSuite+ takes time to start. Is there a way to cut the startup time?

Latest Updated:08/23/2013

Question:

CubeSuite+ takes time to start. Is there a way to shorten the startup time?

Answer:

If CubeSuite+ V1.02.00 or a later version is used, the startup time of CubeSuite+ can be reduced by specifying not to start unnecessary plug-ins with the method below.

In CubeSuite+, select [Tool] menu >> [Plug-in Setting...] to open the Plug-in Manager dialog box. Then, remove the check from the [Basic Function] tab and [Additional Function] tab.

For details, refer to the following manual from here.
Plug-in Manager dialog box, in
APPENDIX A, WINDOW REFERENCE, in
CubeSuite+ Integrated Development Environment User's Manual: Start

Suitable Products
CS+ (formerly CubeSuite+)