Skip to main content
Knowledgebase
Home
Renesas Electronics Europe - Knowledgebase

Can I use the source code generated by Code Generator tool with real-time OS

Last Updated:03/22/2017

Question:

Can I use the source code generated by Code Generator tool with real-time OS?

Answer:

Note that the Code Generator tool has not been evaluated in use in combination with the real-time OS environment. When using the Code Generator tool, combined with the real-time OS, customers should consider the following use conditions in advance and use those at their own discretion.

1.    The functions and the library generated by Code Generator tool are not the reentrant.
2.    The Code Generator tool does not take into account interrupt processing in the real-time OS.
 

Suitable Products
e² studio
CS+ (formerly CubeSuite+)
Code Generator