Skip to main content
Renesas Electronics Europe - Knowledgebase

Can I use programs compiled in CA78K0R compiler to RL78/78K0R devices?

Latest Updated:04/24/2015


I am using the CC-RL compiler for RL78 devices. Can I use programs compiled with the CA78K0R compiler on RL78 or 78K0R devices?


The CC-RL compiler provides the -convert_cc (as a compiler option) and -convert_asm (as an assembler option) options to aid porting from the CA78K0R to the CC-RL compiler. Specifying these options converts most of the code in the programs for the former compiler so that they can be handled by CC-RL.
Note, however, that the interface with functions differs in some respects between the CA78K0R and CC-RL compilers. You will need to check the interface if you are using the assembler or have defined assembly functions.
Suitable Products
e² studio
CS+ (formerly CubeSuite+)
C Compiler Package for RL78 Family