Skip to main content
Knowledgebase
Home
Renesas Electronics Europe - Knowledgebase

Why description of the default settings only contains in wsetup.c?

Latest Updated:09/10/2007

Question:

[High-performance Embedded Workshop V.4]  When building a project, wsetup.c only contains description of the default settings for particular modules. Why?

Answer:

hwsetup.c is a file with has a function make the default settings of UPU.

Since the default settings of CPU depend on system, there're so many settings and High-performance Embedded Workshop can't support every cases. So, we described a coding example of the default settings using the commonly used module.

Please modify hwsetup.c according to your developping system.

Suitable Products
High-performance Embedded Workshop