Skip to main content
Renesas Electronics Europe - Knowledgebase

Is the no. of cycles reflected to external memory's number of states?

Latest Updated:09/10/2007


Is the number of cycles which are displayed by performance analysis reflected to the external memory's number of states which is set into the control register?


No. It does not reflect the control register settings. The number of cycles is calculated depending on the number of states set by the memory map.
Suitable Products
High-performance Embedded Workshop
Simulator Debugger for SuperH Family [for High-performance Embedded Workshop]
Simulator Debugger for H8SX, H8S, and H8 Families [for High-performance Embedded Workshop]