Skip to main content
Knowledgebase
Home
Renesas Electronics Europe - Knowledgebase

Errors occur in setting external flash ROM using external flash editor

Latest Updated:12/05/2014

Question:

I use the E1/E20 emulator for the RX microcomputer.
I set the external flash ROM by using an external flash definition editor, but when I downloaded a program to it, the error message below was displayed and correctly writing the program was not possible.

CubeSuite+:
An error has occurred in verification of the external flash ROM. The flash ROM may have been degraded. (E1812802)
or
An error has occurred in erasing of the external flash ROM. The flash ROM may have been degraded. (E1812800)

High-performance Embedded Workshop:
An error has occurred in verification of the external flash ROM. The flash ROM may have been degraded.
or
An error has occurred in erasing of the external flash ROM. The flash ROM may have been degraded.

Answer:

The error might be occurring because the case described in the issue of tool news shown below is applicable.
http://tool-support.renesas.com/eng/toolnews/110816/tn2.htm

The tool news above describes a countermeasure for use with the High-performance Embedded Workshop. If you are using CubeSuite+, carry out the operations below.

  1. Recreate a USD file after selecting the lock function.
  2. Select [No] for [Erase external flash ROM before download] in the CubeSuite+ properties panel.
Suitable Products
CS+ (formerly CubeSuite+)
High-performance Embedded Workshop
E1 [R0E000010KCE00]
E20 [R0E000200KCT00]