Skip to main content
Knowledgebase
Home
Renesas Electronics Europe - Knowledgebase

Can I install CubeSuite+ on a PC using CC-RX where HEW is installed?

Latest Updated:10/28/2014

Question:

I'm using the CC-RX compiler.
Is it possible to install CubeSuite+ on a PC on which the High-performance Embedded Workshop is already installed ?

Answer:

There are versions of the CC-RX compiler for the High-performance Embedded Workshop and CubeSuite+.
Both environments can be installed on the same PC because the versions of CC-RX for the different environments are installed in separate directories.
Suitable Products
CS+ (formerly CubeSuite+)
High-performance Embedded Workshop
C/C++ Compiler Package for RX Family