Skip to main content
Knowledgebase
Home
Renesas Electronics Europe - Knowledgebase

Why does New Update Available appears if I use AutoUpdate Utility?

Latest Updated:05/14/2007

Question:

Although I used the AutoUpdate Utility to update to Flash Development Tool Kit V.3.07 Release 01, the "New Update Available" message still appears on the screen.

Answer:

This problem occurs when the update programs for both Flash Development Tool Kit V.3.07 Release 01 and AutoUpdate Utility are installed on a computer that is also installed with AutoUpdate Utility V.1.01 Release 00.

Solution: Close the AutoUpdate Utility, go to "Add & Delete Programs" in the Windows control panel, select "Renesas AutoUpdate Utility" and delete the AutoUpdate Utility. After you delete the utility, download and reinstall the AutoUpdate Utility from the Renesas Homepage.

Suitable Products
Flash Development Toolkit