Skip to main content
Knowledgebase
Home
Renesas Electronics Europe - Knowledgebase

Why can't I write in Intel HEX format with M3T-ICC740 to the target MCU?

Latest Updated:06/15/2009

Question:

I am using the Flash Development Toolkit but I can't write the Intel HEX format file I created with M3T-ICC740 to the target MCU. What could be the problem?

Answer:

The Flash Development Toolkit does not support the write operation for Intel HEX format files. We recommend you convert the file to Motorola S record format.

  • V.1.01 Release 02 and newer versions of M3T-ICC740
    The file with the .mot extension generated in the project folder is the Motorola S format. Use this file for the write operation to work around this problem.
     
  • V.1.01. Release 01 and older versions of M3T-ICC740
    Because the following options are specified in the linker by default, a Hex file (Intel format) as a absolute load module is created.
        -o "$(CONFIGDIR)¥$(PROJECTNAME).hex" -Fintel-standard -Y0
    To create a Motorola S format file, change the above as follows:
        -o "$(CONFIGDIR)¥$(PROJECTNAME).mot" -Fmotorola.
Suitable Products
C Compiler Package for 740 Family [M3T-ICC740]
Flash Development Toolkit