Skip to main content
Knowledgebase
Home
Renesas Electronics Europe - Knowledgebase

Which device name I should select in [Device and kernel selection]?

Latest Updated:06/23/2011

Question:

[Flash Development Toolkit V.3, V.4]I cannot find the device name I wish to use in [Device and kernel selection] window when creating project. Which device name I should select?

Answer:

Confirm that your Flash Development Toolkit supports the target device by referencing the Supported Device Table below. Select the device name as listed in the “Select Device” example in the [Device and kernel selection] window.

For Flash Development Toolkit V.4, click here.

For Flash Development Toolkit V.3, click here.
Suitable Products
Flash Development Toolkit