Skip to main content
Knowledgebase
Home
Renesas Electronics Europe - Knowledgebase

Does development environment for 740 family MCUs support Windows 7?

Latest Updated:08/24/2016

Question:

Does the development environment for the 740 family MCUs support Windows 7?

Answer:

Please refer to the information on the “Compatibility of Renesas Software Tools with Microsoft Windows® 7” page at the URL below and click on the link “Development Environment of 740 Family” to check on the state of support for Windows 7 by the development environment for the 740 family MCUs.

http://tool-support.renesas.com/autoupdate/support/eng/windows/7/index.html
Suitable Products
High-performance Embedded Workshop
Auto Update Utility
Install Manager
C Compiler Package for 740 Family [M3T-ICC740]
Assembler Package for 740 Family [M3T-SRA74]
Simulator Debugger for 740 Family [M3T-PD38SIM]
E8a
M38000T2-CPE
Flash Development Toolkit