Skip to main content
Knowledgebase
Home
Renesas Electronics Europe - Knowledgebase

Can you tell me the operating environments of FDT?

Latest Updated:04/05/2005

Question:

[Flash Development Toolkit V.2, V.3, V.4] Can you tell me the operating environments of Flash Development Toolkit?

Answer:

We recommend the following operating environments to use the Flash Development Toolkit.

  • Host computer:Compatible machine with IBM PC (Pentium 800MHz or more)

  • Memory capacity: Minimum 128MB (256MB or more recommended)

Suitable Products
Flash Development Toolkit