Skip to main content
Renesas Electronics Europe - Knowledgebase

Product Fluctuate: if AC & DC defines minimum and maximum values?

Latest Updated:04/01/2008


DC and AC characteristics define the minimum and maximum values. Does this mean that the characteristics of a product fluctuate?


No, it does not. The meaning is different between input and output.
The minimum and maximum values of the output are characteristics peculiar to the product and mean that variations of each product are within the range.
The values of the input refer to an allowable range.
These characteristics of some devices change depending on the temperature, power supply, and input voltage, but the specified range of the minimum and maximum values is not exceeded under the condition of operation within the guaranteed range.
Suitable Products