Skip to main content
Knowledgebase
Home
Renesas Electronics Europe - Knowledgebase

Is data area set by SBK& RBK valid until next instructions are executed?

Latest Updated:11/12/2004

Question:

(CPU)   Is reference data area set by the SBK and RBK instructions valid until the next SBK and RBK instructions are executed? [2004/11/12]

Answer:

Yes. However, after reset or exiting from power-down mode, pages 0 to 63 are set. (#105053)
Suitable Products
455A
4571