Skip to main content
Knowledgebase
Home
Renesas Electronics Europe - Knowledgebase

If SI/O3 & SI/O4 set at receive only, can SOUTi pin be used as an I/O port?

Latest Updated:09/22/2010

Question:

If SI/O3 and SI/O4 are set for receive only, can the SOUTi pin be used as an I/O port?

Answer:

When SI/O3 and SI/O4 are set for receive only, the SOUTi pin can only be used as an input port (it cannot be used as an output port). When using as an input port, set the SMi2 bit in the SiC register to "1".
Suitable Products
M16C/62A
M16C/62A(M16C/62T)
M16C/62M
M16C/62N
M16C/62N(M3062GF8NFP, M3062GF8NGP)
M16C/62P
M16C/63
M16C/64A
M16C/64C
M16C/65
M16C/65C
M16C/29
M16C/28