Skip to main content
Renesas Electronics Europe - Knowledgebase

How to operate switching regulator circuit as mentioned in manual?

Latest Updated:11/01/2005


I designed my switching regulator circuit according to the description in the manual, but it still won't operate.


Check the following.

  • Is there any incorrect wiring?
  • The GND wiring can sometimes be a cause of malfunction. Make sure that the GND pins for signal lines and power lines are separate, and that each is grounded to a separate point.
  • Is there a capacitor connected between the VREF (REFERENCE, REF) and GND pins? If so, be sure to use a film, tantalum, or ceramic capacitor.
Suitable Products
Power Management Linear