Skip to main content
Knowledgebase
Home
Renesas Electronics Europe - Knowledgebase

What are drooping characteristics output of a 3-terminal regulator?

Latest Updated:12/01/2011

Question:

What are the drooping characteristics of the output of a 3-terminal regulator?

Answer:

They can be easily calculated from the IOpeak-(VIN-VO) characteristics.
Suitable Products
CMOS Operational Amplifiers
Bipolar Operational Amplifiers
3 Terminal Regulators