Skip to main content
Knowledgebase
Home
Renesas Electronics Europe - Knowledgebase

For the UPC2800A, how do I adjust the reception sensitivity?

Latest Updated:12/01/2011

Question:

For the UPC2800A, how do I adjust the reception sensitivity?

Answer:

The reception sensitivity can be adjusted by externally attaching a resistor to pin 7.
Suitable Products
  • Was this article helpful?