Skip to main content
Knowledgebase
Home
Renesas Electronics Europe - Knowledgebase

What are the thermal resistance of 2SK1285?

Latest Updated:09/02/2013

Question:

For the 2SK1285, what are the channel to case thermal resistance (Rth(ch-c)) and the channel to air thermal resistance (Rth(ch-a))?

Answer:

Thermal resistance of the 2SK1285 is as follows.

  • Channel to case thermal resistance, Rth(ch-c): 6.25 ℃/W
  • Channel to air thermal resistance, Rth(ch-a): 96.15 ℃/W
Suitable Products
Power MOSFETs for General Switching