Skip to main content
Renesas Electronics Europe - Knowledgebase

How to measure the gate to drain & source leakage current of NP84N075?

Latest Updated:09/02/2013


When I measure the gate to drain and gate to source leakage current of the NP84N075, they are quite small compared to the specs in the datasheet (MAX. ±100 nA). I wonder if my measuring method is incorrect.


The MAX value is a specified value. Please refer to TYP for an actual value. Depending on the accuracy of the measuring method and measurement device, measurement error may also be possible.

This article is written based on not recommended products.

Suitable Products
Power MOSFETs for General Switching