Skip to main content
Knowledgebase
Home
Renesas Electronics Europe - Knowledgebase

Are there any n-channel MOSFET with similar characteristics?

Latest Updated:09/02/2013

Question:

I'm looking for a MOSFET to use for power amplification in the latter part of an operational amplifier (op-amp). I would like to develop a ±300 V amp using p-channel and n-channel. Please suggest complementary p-channel and n-channel MOSFETs with matching characteristics. I'm considering using the 2SJ181 for p-channel. Is there an n-channel MOSFET with similar characteristics?

Answer:

The RJK6032DPD n-channel MOSFET has similar switching characteristics to the 2SJ181S. Please consider it.
Suitable Products
Power MOSFETs for General Switching