Skip to main content
Knowledgebase
Home
Renesas Electronics Europe - Knowledgebase

What is Zener diode?

Latest Updated:09/01/2006

Question:

Zener diode

Answer:

(Zener diodes are named in accordance with Renesas Electronics' original naming format.)
The Orderable Part Number is explained below using the RD Series as an example.

Suitable Products
  • Was this article helpful?