Skip to main content
Knowledgebase
Home
Renesas Electronics Europe - Knowledgebase

What is Depletion?

Latest Updated:11/01/2005

Question:

Depletion

Answer:

This is a type of MOS FET. A depletion type MOS FET has a characteristic that the drain current flows when the gate voltage is 0 V.
Today, enhancement type MOS FETs are generally used.
Products are ranked by the current when the bias is zero.
Suitable Products