Skip to main content
Renesas Electronics Europe - Knowledgebase

How many channel does ICC value of operational amplifier indicate?

Latest Updated:12/01/2011


How many channels' current does the circuit current (ICC) value of an operational amplifier indicate?


The circuit current value indicates the total for all channels incorporated in a single package (2 channels: dual type; 4 channels: quad type). Note that this value is calculated assuming there is no load on any channel; in other words, a current that flows through the power supply pins when the output current is 0 A is assumed.

Suitable Products
Operational Amplifiers
USB2.0 Host/Peripheral Controller