Skip to main content
Knowledgebase
Home
Renesas Electronics Europe - Knowledgebase

Are there any difference among B1, B2, and B3 ranks?

Latest Updated:04/01/2006

Question:

The RD27S rank is only indicated as "B" in the data sheet, but the marking on the actual product shows "B1". Is there actually any difference between B1, B2, and B3 ranks?

Answer:

No, it has no difference. The RD27S rank is only "B".
The "1" in the "B1" is marked only for convenience.
Suitable Products
  • Was this article helpful?