Skip to main content
Knowledgebase
Home
Renesas Electronics Europe - Knowledgebase

Crossover Distortion Generate: if audio signal expand with uPC358

Latest Updated:12/01/2011

Question:

Crossover distortion is generated in the output when an audio signal is amplified with the uPC358.

Answer:

Yes, this is correct.
If the crossover distortion is a problem, use the uPC1458 or the uPC4572 for audio applications, or else use the uPC4742, which does not generate crossover distortion.
Suitable Products
Operational Amplifiers
USB2.0 Host/Peripheral Controller
M66596, R8A66597
UPD720150