Skip to main content
Knowledgebase
Home
Renesas Electronics Europe - Knowledgebase

Do you have ESD protection diodes for data lines?

Latest Updated:11/01/2005

Question:

Do you have ESD protection diodes for data lines?

Answer:

Yes, we have the NNCD Series and NSAD Series.
The NSAD Series in particular consists of diodes that have developed for high-speed data lines such as USB2.0, IEE1394a, DVI, and 100B.
For details on these series, visit the following links.

•NSAD Series Features
•NNCD Series Features
Suitable Products