Skip to main content
Knowledgebase
Home
Renesas Electronics Europe - Knowledgebase

What are the temperature characteristics of hFE?

Latest Updated:03/01/2006

Question:

What are the temperature characteristics of hFE?

Answer:

The temperature characteristics of hFE are (approx.) 0.5 to 1.5%/°C. When designing your circuit, be sure to make allowances for a drop in hFE, especially at low temperatures.
Suitable Products
Diodes for Constant Voltage
RKZ-KD Series
HZ Series
HZS Series
HZ-P Series
HZ(H) Series
HZT Series
HZU Series