Skip to main content
Knowledgebase
Home
Renesas Electronics Europe - Knowledgebase

Can a comparator be used as an operational amplifier?

Latest Updated:12/01/2011

Question:

Can a comparator be used as an operational amplifier?

Answer:

Yes, but because comparators do not incorporate a phase compensation capacitor, oscillation will occur when negative feedback is applied. It is therefore impractical to use a comparator as an operational amplifier because a large-capacity capacitor must be connected to the output, slowing the speed considerably.

Suitable Products
Comparators