Skip to main content
Knowledgebase
Home
Renesas Electronics Europe - Knowledgebase

TPS-1 Variable "L" in SPI Slave Interface

Last Updated:06/01/2017

Question:

What is the variable "L" in the TPS-1 user's manual in regards to the "SPI Slave Interface Handshake Wait"?

Answer:

"L" is the time between "end of of transfer" and subsequent "beginning of transfer".
Suitable Products
TPS-1
  • Was this article helpful?