Skip to main content
Knowledgebase
Home
Renesas Electronics Europe - Knowledgebase

TPS-1 SPI Clock for Flash Interface

Last Updated:06/01/2017

Question:

Can the customer change the clock of the SPI flash interface?

Answer:

The clock is set by the firmware and cannot be changed by the customer.
Suitable Products
TPS-1
  • Was this article helpful?