Skip to main content
Knowledgebase
Home
Renesas Electronics Europe - Knowledgebase

TPS-1 PROFINET Stack V1.3 Multiple Write

Last Updated:06/02/2017

Question:

The PROFINET stack V1.3 and before cannot handle the “MultipleWrite” package from the master, so TPS-1 could not connect with it. How do I work around that?

Answer:

The PROFINET stack V1.3 and earlier cannot handle multiple writes. To avoid problems with this restriction, we recommend changing the GSDML file. Change the “MultipleWriteSupported = true” to MultipleWriteSupported="false" or just update the stack to V1.4 or later.
Suitable Products
TPS-1
  • Was this article helpful?