Skip to main content
Knowledgebase
Home
Renesas Electronics Europe - Knowledgebase

TPS-1 PROFINET Stack Updates

Last Updated:06/02/2017

Question:

Can the stack be updated if the next generation of PROFINET is released?

Answer:

The PROFINET stack running on TPS-1 can be updated with each generation of PROFINET.
Suitable Products
TPS-1
  • Was this article helpful?