Skip to main content
Knowledgebase
Home
Renesas Electronics Europe - Knowledgebase

TPS-1 Firmware Updates via Host MCU

Last Updated:06/01/2017

Question:

Can the TPS-1 firmware be updated by a host MCU?

Answer:

Yes, the software driver includes the APIs to do this.  Please refer to “Firmware Update Over Host Interface” in the TPS-1 toolkit driver manual.
Suitable Products
TPS-1
  • Was this article helpful?