Skip to main content
Knowledgebase
Home
Renesas Electronics Europe - Knowledgebase

PROFINET Stack Version for TCP/IP Ethernet Support

Last Updated:06/02/2017

Question:

Starting at which PROFINET stack version will standard TCP/IP Ethernet be supported?

Answer:

Standard TCP/IP Ethernet is supported from PROFINET stack version 1.1 onwards. From this version onwards the customer has the possibility to send or receive TCP/IP frames via the API driver. The transmission of TCP/IP frames is possible without a PROFINET controller but the TCP/IP stack must then be implemented on the host CPU under the responsibility of the customer.
Suitable Products
TPS-1