Skip to main content
Knowledgebase
Home
Renesas Electronics Europe - Knowledgebase

PROFINET Stack Version for Optical Interfaces

Last Updated:06/02/2017

Question:

Starting at which PROFINET stack version will optical interfaces be supported?

Answer:

Optical interfaces are supported from PROFINET stack version 1.1 onwards.
Suitable Products
TPS-1