Skip to main content
Knowledgebase
Home
Renesas Electronics Europe - Knowledgebase

What are the package dimensions for Synergy devices?

Latest Updated:10/13/2016

Question:

What are the package dimensions for Synergy devices?

Answer:

The PDF package drawings for each device are included in the device User's Manuals. You can find links to all the Synergy Device Use's Manual's on the Synergy MCU web page by selecting the Documentation Tab:

https://www.renesas.com/produc...ntrollers.html 

  • Was this article helpful?