Skip to main content
Renesas Electronics Europe - Knowledgebase

tx_src Module Guide Resources

Last Updated:03/01/2018


Where can I find the module guide resources for the ThreadX Source module on tx_src?


Information on the module guide itself and the associated resources and known issues are available here.


The ThreadX Source Module provides configurable options for a wide range of ThreadX properties. These include properties for:

  • Timer settings
  • Stack settings
  • Priority settings


Module Guide

The ThreadX Source module guide is targeted for SSP 1.2.0 and above.

The ThreadX Source module guide is available here.

Module Guide Resources

The following useful user manuals are included in the X-Ware documentation package available here.

  • ThreadX User’s Manual


Known issues

  • Refer to the SSP release notes for known issues, available here.


Suitable Products
  • Was this article helpful?