Skip to main content
Renesas Electronics Europe - Knowledgebase

sf_power_profiles Module Guide Resources

Last Updated:11/21/2017


Where can I find the Power Profiles framework module guide resources for the sf_power_profiles module?


Information on the module guide itself and the associated resources and known issues are available here.


The Power Profiles Framework is a generic API that can be configured to allow the MCU to be placed in lower power Software Standby mode. The module is implemented on sf_power_profiles.

The Power Profiles Framework has the following features:

  • Supports Software Standby operations
  • Supports multiple operating modes
    • Run
    • RTC
    • External Interrupt
  • Selects clocks and peripherals to disable during Software Standby
  • Selects output pin state prior to and after exiting Software Standby

Module Guide

The Power Profiles Framework module guide is targeted for SSP 1.2.0 and above and the SK-S7G2 Kit.

The Power Profiles Framework module guide application note, application project and import guide are not yet available.

Module Guide Resources

  • Content provided as it becomes available.

Known issues

  • Refer to the SSP release notes for known issues, available here.


  • Was this article helpful?