Skip to main content
Knowledgebase
Home
Renesas Electronics Europe - Knowledgebase

sf_el_nx_comms Module Guide Resources

Last Updated: 02/28/2018

Question:

Where can I find the resources for the Communications Framework on NetX module guide resources?

Answer:

Information on the module guide itself and the associated resources and known issues are available here.

Introduction

The Communications Framework on NX provides high-level APIs for Communications Framework applications and is implemented on NetX Telnet. The Communications Framework uses the Ethernet peripheral on the Synergy MCU.

The Communications Framework has the following features:

  • High level connectivity is supported on Ethernet but is easily changed to UART and USB connectivity without API modification
  • Supports channel locking for exclusive access
  • Thread aware implementation uses mutex and event flags internally

Module Guide

The Communications Framework on NX module guide is targeted for SSP 1.2.0 and above and the SK-S7G2 Kit.

Currently there is now module guide for the Communications Framework on NX module.

Module Guide Resources

  • Content provided as it becomes available.

Known issues

  • Refer to the SSP release notes for known issues, available here.
Suitable Products
SSP
  • Was this article helpful?