Skip to main content
Renesas Electronics Europe - Knowledgebase

sf_block_media_ram Module Guide Resources

Last Updated:02/28/2018


Where can I find the references to module guide resources for the Block Media RAM Framework module on sf_block_media_ram?


Information on the module guide itself and the associated resources and known issues are available here.


The Block Media Framework Module implements a file system on RAM for read, write, and control of the read/write region of RAM memory. The framework has all the functionality needed to interface with a file system through a block media interface.

The Block Media RAM Framework module supports the following features:

  • Enable FileX to be run on linear memory-mapped devices.
  • Temporary and fast storage of data on RAM.


Module Guide

Currently there is no module guide available for this module.


Module Guide Resources

Resources will be added as they become available. 


Known issues

  • Refer to the most current SSP release notes for any known issues.
Suitable Products
  • Was this article helpful?