Skip to main content
Knowledgebase
Home
Renesas Electronics Europe - Knowledgebase

sf_block_media_qspi Module Guide Resources

Last Updated:02/28/2018

Question:

Where can I find the references to module guide resources for the Block Media QSPI Framework module on sf_block_media_qspi?

Answer:

Information on the module guide itself and the associated resources and known issues are available here.

Introduction

The Block Media QSPI Framework Module implements APIs for a QSPI channel and supports read, write, and control of the QSPI Flash memory peripheral through the r_qspi driver. The driver has all the functionality needed to interface with a file system through a block media interface.

The Block Media QSPI Framework module supports the following features:

  • Supports the QSPI channel interface for a QSPI flash memory device.
  • Supports a file system on QSPI flash memory.

 

Module Guide

Currently there is no module guide available for this module.

 

Module Guide Resources

Resources will be added as they become available. 

 

Known issues

  • Refer to the most current SSP release notes for any known issues.
Suitable Products
SSP
  • Was this article helpful?