Skip to main content
Knowledgebase
Home
Renesas Electronics Europe - Knowledgebase

r_jpeg_decode Module Guide Resources

Last Updated:03/26/2018

Question:

Where can I find the module guide resources for the JPEG HAL module on r_jpeg_decode?

Answer:

The JPEG Decode HAL module doesn't currently have its own module guide. It is included in the sf_jpeg_decode module guide. The resources article for the sf_jpeg_decode module is available here.
SSP
  • Was this article helpful?