Skip to main content
Knowledgebase
Home
Renesas Electronics Europe - Knowledgebase

r_fmi Module Guide Resources

Last Updated:11/22/2017

Question:

Where can I find the references to module guide resources for the FMI HAL module on r_fmi?

Answer:

Information on the module guide itself and the associated resources and known issues are available here.

Introduction

The FMI HAL module is a high-level API for applications that read records from the Factory MCU Information Flash Table. The FMI HAL module is implemented on r_fmi. The FMI HAL module uses the Flash Interface on the Synergy MCU.

The FMI HAL modules support the following features:

  • Product Information- such as Product Name, Package, Pin count, and Temperature range
  • Product Features- such as Version major, Version minor, and Variant data
  • Event Information- such as Interrupts and Events

Module Guide

The FMI HAL module guide is targeted for SSP 1.2.0 and above and the SK-S7G2 Kit.

The most recent versions of the FMI HAL module guide application note, application project and import guide are available here.

Module Guide Resources

  • The FMI HAL module is used in the Developer Examples for the DK-S7G2. You can find a Knowledge Base article that describes the Developer Examples and how to create a project using the template here.

Known issues

  • Refer to the SSP release notes for known issues, available here.

SSP

  • Was this article helpful?