Skip to main content
Knowledgebase
Home
Renesas Electronics Europe - Knowledgebase

Why do I have an issue when compiling ThreadX source with ISDE v5.0.0.024 and SSP v1.1.0-alpha.1 for the S124?

Latest Updated:10/13/2016

Question:

Why do I have an issue when compiling ThreadX source with ISDE v5.0.0.024 and SSP v1.1.0-alpha.1 for the S124?

Answer:

When you add tx_src from the configuration tab in an S124 project you will get a compile error. There is no current work around, but this issue will be fixed in the next release.